Solution
Automotive Window Pinch Force Testing
An automotive manufacturer needs a force testing system for their vehicle power windows
An automotive manufacturer needs a force testing system for their vehicle power windows. They want to prevent any injuries or other safety concerns by testing the strength of pinch force of their power windows.
Interface’s SML Low Height S-Type Load Cell can be placed in between the power window and the door frame. Two plates are attached to the top and bottom of the SML with LB Load Buttons. As the power window pinches the SML load cell, force results are sent and displayed using the 9870 High-Speed High Performance TEDS ready Indicator.
The automotive manufacturer was able to successfully determine the force strength of their power windows.
Notifications